Part Number: LMX2595
Hello team,
My customer has a question about LMX2595. Could you please confirm this?
rb_VCO_DACISET value reaches upper limit of 511 and Vtune voltage becomes about 0.8V when changing frequency from around 13GHz(higher frequency in VCO SEL=5) to other frequency(e.g. 9GHz, 10GHz and 11GHz) with No Assist mode.
In this condition, VCO_DACISET_STRT=300 is used as recommended in datasheet.
If changing the VCO_DACISET_STRT to 200, then customer can get normal rb_VCO_DACISET value and Vtune voltage.
Questions are
- Is the rb_VCO_DACISET=511 condition expected as normal operation?
- Although reducing VCO_DACISET_STRT to 200 seems improve the situation, is it right solution?
- If above can be solution, could you let me know recommended VCO_DACISET_STRT value for each frequency?
Best regards,