This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq4822y issues

Hello

We use the bq4822y RTC.  During stress testing (real time clock reads in a tight loop) we can occasionally read values that are not valid.  (i.e seconds larger than 59, months equal to zero etc..)  Sometimes the internal registers will retain this bad value and the chip nees a new time written to it to correct it.  This bad value will be retained even after a power off condition.  Is there any kind of restrictions as to how fast user can read the clock?

To prevent reading data in transition the read bit D6 of the control register is set to 1.  After reading this bit is cleared.

RR

  • Hi Russell,

    Start by verifying that the logic levels meet the specifications for High voltage and Low voltage levels.  Also, negative voltage levels may corrupt the data.

    The frequency of reads will depend on the steps taken during the multiple reads (Address Enable time, Chip Enable time, Output Enable time).  These times are in the 10ns to 70ns range. The table is listed on page 10 of the datasheet.