This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: phase noise of some frequency do not match the datasheet of LMX2594

Part Number: LMX2594


Hi, i am using LMX2594 as a LO in my frequency synthesizer. I find that phase noise of some frequency do not match the datasheet of LMX2594.Here are my circuits  and testing results.

LMX2594 works in the fractional mode. I want to get 8780~8789MHz, 8880~8889MHz, 8980~8989MHz and etc, with 1MHz step.

Why the phase noise of 8789MHz is worse than that of 9789MHz?

Thank you!