Part Number: LMK04828
We are using LMK04828B device on our board with two oscillators. 10 MHz for reference of PLL1 and 100 MHz for PLL2. However due to bad performance of 100 MHz oscillator (has lots of harmonics) performance of LMK device degredes. Is there a way to bypass 100 MHz OSCin clock and generate final output clocks (2400 MHz) from 10 MHz reference clock? If so what is the configuration for this option?