Hello,
We have several LMX2594 devices on multiple boards. Below is the configuration
Osc_in: 122.88 MHz
RFOutA, RFOutB: 3932.16MHz
In order to get all RFOut* signals phase aligned (from all devices on multiple boards), do I need to use SYNC pin? If yes, can it be a continuous clock running at 7.68MHz? or it must be a single pulse?