Part Number: LMK04828
Hello,
Although LMK04828 has many kind of Vcc rails, are those Vcc rails can be powered up in any order?
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04828
Hello,
Although LMK04828 has many kind of Vcc rails, are those Vcc rails can be powered up in any order?
Best regards,
K.Hirano
Hello Hirano-san,
The VCC rails may be powered up in any order.
Once the VCC rails are powered up and stable, the device should be reset by writing 1 to the RESET register (R0[7]) or by asserting HIGH signal on the reset pin, and then all registers should be programmed. The datasheet recommended programming sequence (section 9.5.1) is a good example to follow.
Regards,