Other Parts Discussed in Thread: MSP430FR2000, SN74HCS72-Q1, SN74LVC1G123
Greetings to all,
Hi, I have a mini project that needs to me design a circuit that detect pulse width of 10% and 20%, with input signal of 10ms clock period signal. Second of part of the project is to convert the 10% input pulse width to 60% and generate 5V if the circuit detected 20% input pulse width.
I do know that I have to use 555 timer to convert the duty cycle but I am having trouble designing the pulse width detector. My approach is to use a counter to detect the input pulse width, is that correct?