Part Number: BQ4802LY
i'm working on a retro project that requires an older TI based real time clock chip (BQ4847YMT) as it has the need to control external SRAM.
I see that the BQ4802LY has this ability, but doe not have a built in crystal. I am wondering if this chip is compatible for the functionality to replace the BQ4847YMT? I know I will need to build an adapter board to solder the chip and a crystal to if it is.
Can anyone tell me if this RTC will work or is there a better selection from a new active chip for me to use?
The original BQ4847 datasheet is attached.