Part Number: LMK04832
Other Parts Discussed in Thread: LMK05318, LMK04806,
The datasheet does not specify the amount of decoupling for the LMK04832, i.e. how much, values of capacitors etc ....
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rajan,
Please take a look at the schematic provided in https://www.ti.com/lit/ug/snau215a/snau215a.pdf. The populated capacitors, should be enough.
Thanks,
Vibhu
Hello,
Can the LMK04832 be configured to output a clock as soon as it is powered-up without the need to program it using its SPI interface?
Kind Regards,
Rajan
Hello Rajan,
No the LMK04832 does not have an EEPROM or ROM to enable this.
Some of our commercial parts such as the LMK05318 have this feature.
I will get back to you regarding the schematic.
Thanks,
Vibhu
Hello Rajan,
Following up on the schematic and power supply capacitors. To understand the decoupling caps and ferrite beads needed a good source is section "10 Power Supply Recommendations" and "Figure 40. Example Application – Power System Schematic" of the LMK04806 datasheet. This explains some concepts of why certain capacitors and ferrite beads are necessary. Keep in mind that the VccXs are jumbled between the parts and this is not an apples to apples comparison. For example: on the LMK04806 Vcc4 is the digital supply while on the LMK04832 Vcc5 is the digital supply.
I think Figure 40 on this datasheet should be a good reference when looking at simultaneously with the LMK04832EVM I pointed to before. Here are some of the key points I'd like to point out on the LMK04832:
I do not see any issues with the LMX device, I looked through the unused pins briefly, they seem to be terminated correctly, if you haven't already maybe compare them with section "Table 11. Recommended Treatment of Pins" of the datasheet to double check that you have the functionality you require. The caps to Vcc and GND seem to have followed the EVM.
For future reference please do not share confidential information on e2e as this is a public forum, please contact the field engineer who supports you for sensitive inquiries.
Thanks,
Vibhu
Hello Rajan,
This is what we use on our EVMs:
MMZ1005Y121CT000
Ferrite Bead, 120 ohm @ 100 MHz, 0.4 A, 0402
Ferrite beads with excessive impedance at high frequency (> 200-ohm) can degrade crosstalk performance, especially on the output and SYSREF supplies.
Thanks,
Vibhu