Part Number: LM555
Dear Sir/Ms.
My client uses LM555 to generate 40% Duty but his actual result is 60% Duty. The customer said that he adjusted the resistance ratio of RP1 to RP2, the maximum duty is only 50%. The customer's schematic is like an attachment, can you help the customer to see if there are design errors?
SCHEMATIC1 PWM & 3_3V circuit.pdf
Best Regards,
Kami Huang