This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2615-SP: Min Max Frequency

Part Number: LMX2615-SP

We are using the LMX2615-SP to cover a wide frequency range.  What is the minimum and maximum VCO frequency that can be programmed?  The TICS Pro - LMX2615 tool says the minimum VCO frequency is 7620MHz, but the PLLatinum Sim tool and data sheet indicate the minimum is 7600MHz.  The TICS Pro - LMX2615 tool says the maximum VCO frequency is 15240MHz, but the PLLatinum Sim tool says the maximum is 15200MHz.  I am not sure what the VCO limits are.

  • Hello Bill,

    Please refer to the datasheet limits.  The datasheet min max are values that have been verified through characterization and validation.

    I appreciate the feedback on the TICSPro GUI not being aligned with datasheet so we can update in future revision.

    Kind Regards,