Hello team,
I have a question about read back function when full assist mode.
In full assist mode, can the device read back properly from R110, R111 and R112 the values of VCO_DACISET, VCO_CAPCTRL, VCO_SEL which are set in R16, R19 and R20?
According to customer's experiment, VCO_SEL is correctly read, however others are not.
Changing clock speed for the read back gives some improvement but not 100%.
So I would like to know if the device supports the read back in full assist mode.
Best regards,