Part Number: LMK05028
Hi Timothy T
I still have this problem with input 1PPS like descript at https://e2e.ti.com/support/clock-and-timing/f/48/p/838212/3124029?tisearch=e2e-sitesearch&keymatch=LMK05028#3124029
Currently, I using LMK05028 to synchronize with 1PPS from Module GPS
Our setup as attack file TCS:
- XO: 48MHz +-50ppm
- OCXO: 10MHz +-10ppb
- Input 1PPS from module NEO-M8T
- Output: Out 6_245.76MHz from DPLL1, Out_1_ 156.25MHz from DPLL2
- REF Loop bandwidth: 0.02Hz
- TCXO Loop bandwidth 200Hz
We are able to look to 1PPS and have stable output clock but in initial the output frequency jump back and forth a lot the delta about +-500khz
Please take a look at video link below.
https://1drv.ms/v/s!ApxkmBVHw831jsFGyfpXsU9VH0RN2w
Please help me fix this problem
Thanks