This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: First calibration fails after POR

Part Number: LMX2594

Hi,

Our customer's LMX2594 does not lock the PLL on the first calibration after powering on. Recalibrate and it will succeed.
It is set according to "7.5.1 Recommended Initial Power-Up Sequence".
What should I check to find out the cause?
Settings info 
Fosc = 150MHz
Fpd = 150MHz
RFoutA 7000MHz
RFoutB  Power down
Fvco = 14000MHz
Best regards,
Hiroshi