This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2615-SP: Fractional Simplification

Part Number: LMX2615-SP

In using the fractional divider Fnum and Fden, is it required to simplify the Fnum/Fden fraction?  For example say I want to keep Fden = 30 always, and let Fnum vary from 0 to 29.  Is it ok to set Fnum = 15 and Fden = 30, or is it required to simplify the fraction to Fnum = 1 and Fden = 2?  Are there any disadvantages to not simplifying the fraction?

thanks,

Bill

  • Hello Bill,

    The short answer is no, there are no disadvantages in having a bigger denominator.

    The denominator comes into play when you notice spurs which are multiples of:

    phase detector frequency / (k * simplest form of denominator)

    where the simplest form of the denominator is 2 in either case 1/2 or 15/30 and k can be 2,3,4,6 or 12.

    Using a fractional value of 1/2 vs 15/30 will theoretically not change the location or magnitude of the sub-fractional spurs.

    If these spurs are undesired then a fraction such as 10000/20001 can be used, however this will increase the phase noise of the PLL and will have a very small frequency error. The LMX2615-SP does not have a dithering function and this helps us to replicate the same.

    Thanks,

    Vibhu

  • Hi Vibhu,

    It is good that one does not need to simplify the fraction in the divider chain as it simplifies programming especially for broad frequency coverage.

    thanks,

    Bill