Part Number: CDCE913
Hi team,
Could you help to double check whether TI clock pro can program the duty cycle or sync trigger edge singal?
For the selection of a clock generation IC chip, the requirements are as follows:
The working power supply is 3.3V, which supports at least two kinds of frequency output CMOS level (3.3V). One is 2.048MHz (clock signal) and 8kHz (synchronous signal),These two frequencies have the following corresponding relationship, the rising edge of the two shall be aligned, and the 8kHz(synchronous signal) high level cycle includes eight clock signals. (So the duty cycle may not be 50%, how to configure this )
Frequency configuration of the chip: it is also configured through SPI, IIC or UART interfaces
I found the following model cdce913pw on the TI official website. The required frequency can be configured through TI Clock Pro software, but there is no duty cycle and synchronization. I don't know if it can meet my requirements,
If not, please recommend other devices. Thank you for your help