Other Parts Discussed in Thread: LMX2694-EP, LMK04828, LMK04826
Hello,
I am looking to synchronise multiple LMX2594 ICs, and following the flowchart in the datasheet, I think I will require category 3 synchronisation.
Elsewhere on the forum it was mentioned that for such cases it is common to use a SYSREF output from another LMX/LMK product.
Unfortunately there is not much detail on how the SYSREF signal should be generated. Is a single pulse sufficient, or would it require multiple pulses / continuous SYSREF?
What is a typical LMX/LMK that can be used for this purpose?
An additional question I have is whether this all changes if the LMX2594 ICs are on separate PCBs in separate modules?
I am assuming that in that case the SYSREF generators on each PCB would have to be synchronized somehow?
Kind regards,
Wouter