Part Number: LMK03328
Hi
I want to connect the LMK03328 to a clock distributor defined as 1.8V AC LVDS.
The connection is according to the distributor recommendation: a 100nF serial capacitor at the Pos and at the Neg LMK03328 pins, connected to a 100ohm termination between the Pos/ Neg of the receiver (the Clocks distributor) .
However, HyperLynx simulation shows bad SI both at Pre-layout and at Post Layout (the Neg signal looked OK and the Pos signal had several (!) levels which caused the differential signal to look very bad).
I have tried two things:
1. Short the capacitors
2. Move the 100ohm resistor to the left of the serial capacitors
Both attempts ended with much better SI signals.
Can the LMK03328 drive at all a receiver which is "AC LVDS" ?
Can you explain please the above?
How to proceed?
Thanks
Amnnon