This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572: Ramping mode vs phase management

Part Number: LMX2572

Dear Sirs,

i'm studing the possibility to use the LMX2572 such as CW generator.

In my design, I must generate at fixed frequency or stepped frequency.

In the second case, the frequency of the output signal is not constant but
could be changed in up or down with a step of 2 MHz.

I've read the Ramping function of the LMX2572 and I'm verifing this
function for my application.

The questions are:

- Is it possibile to set 2 MHz step when using the Ramping mode, in manual mode;

- When the output frequency of the LMX2572 go from F0 to F0+2Mhz, after rampingclk
signal, is there a specific phase relation between the F0 and F0+2MHz? For example,
when the frequency of output signal change between F0 and F0+2MHz the phase
as constant or it has a jump?

I'm looking forward to hearing from you

Best Regards,
Daniele Sassaroli