This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: output clock problem

Part Number: LMK04832


I am using LMK04832 in signal loop mode. 

1. Set VCO0 to 2500Mhz with OSC input 100Mhz, VCO 1 show lock and CPOUT2 measures abount 1.5V

but on the output clock I need have 6 lvds output clock is 2500Mhz which is same as VCO0 clock, but only few of them give me 2500Mhz as expect, but few of them give me wrong clock output.

if I set divider to 2, and I got 1250Mhz on all 6 channel, so I am sure VCO0 is working, only have problem on some clock when divider set to 1 on some channel.