Part Number: LMK05318
Other Parts Discussed in Thread: LMK05028
Hi all
Would you mind if we ask LMK05318?
The datasheet shows "Zero-Delay Mode (ZDM) Synchronization for 1-PPS Input and Output" on P50.
<Question1>
Zero-delay mode synchronization is for OUTPUT7 only, isn't it?
Is it possible to use this function with other Outputs??
<Question2>
We would like to confirm the setting with LMK05318 on TICSPRO.
There are SYNC Phase Offset(s) and DPLL_REF_SYNC_PH_OFFSET.
What does SUNC Phase Offsets correspond for RXXX?
<Question3>
If DPLL_REF_SYNC_PH_OFFSET is 0 setting, will DPLL1(2) and OUTPUT7 be Zero-delay mode synchronization without phase offset?
<Question4>
There is the description Zero-Delay Mode (ZDM) Synchronization is for 1-PPS Input and Output.
So, in case of Input(Refrence clock) 148.5MHz, is it possible to use ZDM function??
Kind regards,
Hirotaka Matsumoto