Other Parts Discussed in Thread: CDCE62005, CDCE72010, CDCE62002
Hi,
we're using the above TI clock manager CDCE62005 in a project (it also applies to CDCE72010).
After reading the CDCE62002/CDCE62005 SPI related app note I found the MISO line being declared as "open-drain".
This would imply, that the pin has to be pulled up externally via resistor in order to see a high level.
In the mentioned App-Note, the oscilloscope plots for the MISO line indicate a bidirectional behaviour, rather than a open-drain behaviour. (Charging-curve when LE is going high, but "normal" edges on MISO otherwise).
Which is correct? Is the pin open-drain or bidirectional (high impedance when LE is high, actively driving otherwise)?
Best regards,
Jan