Hello,
My customer would like to align RFoutA and RFoutB by SYNC pin.
OSCin, desired RFoutA and RFoutB are as follows.
OSCin = 61.44MHz
RFoutA = RFoutB = 5893.08MHz.
According to Figure 27 of the datasheet, this condition is category 3.
Then, they are stuck at datasheet 7.2.10.3-3. “Determine the value of IncludeDivide:”.
Since desired RFoutA/B = 5893.08MHz, channel divider is 2. But if IncludedDivide=4, VCO frequency gets >20GHz.
So, is it impossible to align RFoutA and RFoutB by SYNC pin in my customer case?
Any workarounds?
Oe, do they have to generate OSCin frequency of which RFoutA/B is integer multiple using anther PLL device prior to LMX2594?
Best regards,
K.Hirano