Part Number: LMK01801
Hi,
I want to divide a ~2.5GHz clock source by 4 using the LMK01801. The datasheet specifies 50 fs additive jitter at 800 MHz (12 kHz to 20 MHz). Is this the case regardless of input frequency and clock division? (Or specified for 800 MHz input divided by 1?)
Are there any more details on the phase noise/jitter characteristics of the LMK1801 available (the only information I can find is from the "Features" section in the top of the datasheet)?
Best regards,
Håkan