This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00304: LMK00304: input range and termination

Part Number: LMK00304


The lmk00304 clock input can accept lvds, lvpecl, cml, ...
lmk00304 differential input voltage swing range is 0.15 ~ 1.3vpp.
The differential input voltage swing range of lvpecl is typical 1.6vpp.
When using lvpecl as the source clock of lmk00304, it seems to exceed the lmk00304 input range (0.15 ~ 1.3vpp).
What should I do if I use lvpecl as the input clock of lmk00304?