This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: Is there a custom field for user in the CDCI6214 EEPROM

Part Number: CDCI6214
Other Parts Discussed in Thread: LMK05318

Hi,

I would like to store a custom data such as the Board Identification Number in the the EEPROM of CDCI6214 without effecting the functionality of the device (I still want to load the PLL configuration from the EEPROM as well). Is this possible? 

Regards