Part Number: LMX2595
Hi. I have few doubts regarding the LMX2595. Can anyone please let me know the following questions
1) As per the data sheet it is recommended that to connect certain values of capacitors and pull up loads ( Inductors and resistors ) to most of the pins connected to the IC . How exactly these values are calculated.
2) For calculating the AC coupling capacitor value what value of impedance is taken (50ohm ??) and what frequency is to be taken, as the value of capacitor depends on the frequency and the mentioned value is 0.1uF for all teh frequencies.
3) What is the switching time of PLL I mean to change from one fixed frequency to another.
4) What is the PLL lockin time to get the stable frequency at the output.
5) What is the maximum power that can be generated at frequencies greater than 15GHz, when it is fed with maximum reference signal input power of +10dBm.
6) I am planning to make the PCB for the LMX2595. What should be the value of trace width for good impedance matching and the copper thickness to be chosen should be either 10mil or 20 mil.
7) Why the designed loop filter, Loop Bandwidth is at 256 KHz and How is it selected?
Any help and answers to my queries would be greatly appreciated.
Thanks in Advance!