Hello
I would like to use the LMK04832 in distribution mode, to transfer high frequency clock (~3GHz) and sysref to DAC. The high frequency clock enters the LMK using CLKin1 input.
Looking on figure 6 on LMK04832 datasheet, it looks like the signal CLKin0 which is used to reset the dividers and generate SYSREF, is actually sampled by the divided signal using the D-flip flop.
So basically I don't need anymore to meet the stringent requirement of the SU and Hold time of the ~3GHz clock, but the much more relaxed timing of the divided signal, up to 8191 division value.
Is that correct?
Thanks