Part Number: LMK04906
Hi team,
The following settings are made when using LMK04906. (Refer to the "Settings for LMK04906" below.)
The following 26 settings are made each time this LMK4906 is actually used.
I'm waiting for 10ms waiting time between 1 and 2, but would you teach the proper value of the waiting time after setting this 1 (R0 INIT) (recommended value by the manufacturer?).
In actual operation, various settings are used many times, so the more the number of uses, the longer the setting time will accumulate, resulting in a longer actual operation time. I'm having a hard time not knowing how to shorten this waiting time.
Settings for LMK04906
1.0x80160200(R0 INIT)
waiting time 10ms
2. ...
...
26. ...
Beat Regards,
Tom Liu