Hi team. What is the residual power at Output A and Output B in POWER DOWN mode (R44[7] or R44[6] is set to 0) reference to maximum output level? The most interest for me is the next combination: Output A in active mode and Output B in PD mode (R44[7]=1, R44[6]=0). What is the residual power at Output B in this case? Is it like Xtalk=-50 dBc (table 6.5 of datasheet)? How it will be changed if at the same time power down external Vcc pullup at Output B?