Part Number: TPL5111
Hello,
I am currently using the TPL5111 in the timer mode in my design.
with the resistor i am using a mosfet which is controlled by a sensor so if we detect the sensor it will connect the delay pin to VDD through the mosfet and set DRVn pin to high.
The problem that the TPL5111 couldn't wake up with the attached resistor ( i am using a 47K so it's about one minutes) after waiting for one minute without the trigger from the sensor it should set the DRVn pin to high and wake up the uC but it doesn't.
If I remove the mosfet it will work normally by detecting the resistor.
I couldn't understand the origin of the problem ( i am using the TPL5111 in timer mode. )
Looking forward to your help. thanks