Part Number: LMX2595
Hello,
Here is my application for Full-Duplex transceiver: for using the PLL + Synth on Up conversion (needs LO range 16 GHz-17.5 GHz) and Down conversion (needs LO range 12.5GHz-13.2GHz) with 100 MHz reference clock. Below are my questions:
1. Can I use the same LMX2595 Microwave PLL Synthesizer to generate LO1 and LO2 as the same time (full-duplex system) for up and down conversion or I have to use two separate chip with 100 MHz reference clock?
2. What is the difference between LMX2595RHAR vs. LMX2595RHAT?
3. For Full-Duplex system, what are the critical points that LO or PLL+Synthesizer need to taking care of?
4. What are the recommendations if it need with two different LO frequencies?
Thanks and hope to receive your advice!