Other Parts Discussed in Thread: LMX2820, LMX2582
Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello JH,
Here are some suggestion for closest solutions.
1. LMX2820: This device can support up-to 1.4 GHz input. There are two channel dividers (binary dividers only) which can support two frequencies. For example: VCO = 9600 MHz, OUT1 = 9600/8 = 1200 MHz, OUT2 = 9600/32 = 300 MHz (not 350 MHz).
2. LMX2582/2592/2594: These devices can support up-to 1.4 GHz input. However, they have one channel divider. You will need to use external frequency divider to generate lower frequency.
3. For 1200 MHz and 350 MHz, it would be two device solution - one for each domain. A splitter can be used to feed 1 GHz input clock to both these devices.
Please let us know any follow-up questions you would have.
Regards,
dinesh.