Part Number: LMK04828-EP
Other Parts Discussed in Thread: LMK04208, LMX2594
Hi Forum,
I'm investigating substituting an LMK04208 in our system for an LMK04828-EP, simply for the expanded temperature range.
Our LMK04208 configuration was producing a clock output of 25.6 MHz for an LMX2594. The product page for the LMK04828-EP says the minimum frequency is 0.001 MHz so I thought this would be an easy substitution. But looking at the minimum VCO frequency and output clock dividers, I can only see getting an output of 2450 MHz / 32 = 76.5625 MHz. Having a peek at the LMK04828B page, I see that you have stated the minimum output frequency as 0.289 MHz, which is the minimum VCO frequency divided by the maximum SYSREF frequency (2370 / 8191 = 0.289...). I'm led to believe that, as for the 04828B, this very low output frequency for the EP model is in fact the lowest SYSREF frequency, and not that of the regular clock output paths.
Is this assumption about the minimum frequency correct? If so, am I limited by the 76.5625 MHz frequency on the clock paths? Is this 0.001 MHz output presuming an external VCO that can operate at far lower frequencies? Am I missing something here?
Also, if its too difficult to make this substitution, is there another LMK product that has the temperature range and a better low output frequency, comparable to the 04208?
Thanks,
Lawrence