Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: CDCE6214, CDCI6214,
I am trying to use the CDCE6214 in I2C mode.
I have REFSEL tied directly to ground so it will power up in operational mode. All the supplies are 2.5V. I am looking for LVCMOS on output0 and LVDS on the other 4. I have 3 prototypes of this system available, they all three behave the same.
PDN, SDA, SCL, HW_SW_CTRL, and GPIO4 are all driven from an FPGA. GPIO1 is also connected to the FPGA, but right now the FPGA has that pin configured as an input.
If I set HW_SW_CTRL='1', GPIO4(OE)='0', then change PDN from '1' to '0'. I can communicate over I2C, I also see power supply current increase.
Here are the register values after PDN is cleared.
0x0053 (d83) = 0xFF00 0x0052 (d82) = 0x05C0 0x0051 (d81) = 0x0004 0x0050 (d80) = 0x0008 0x004F (d79) = 0x0008 0x004E (d78) = 0x0000 0x004D (d77) = 0x0002 0x004C (d76) = 0x0188 0x004B (d75) = 0x8248 0x004A (d74) = 0xA241 0x0049 (d73) = 0x0000 0x0048 (d72) = 0x0006 0x0047 (d71) = 0x0406 0x0046 (d70) = 0x0898 0x0045 (d69) = 0xA241 0x0044 (d68) = 0x0000 0x0043 (d67) = 0x0006 0x0042 (d66) = 0x0006 0x0041 (d65) = 0x4AD8 0x0040 (d64) = 0xA241 0x003F (d63) = 0x0000 0x003E (d62) = 0x0006 0x003D (d61) = 0x0000 0x003C (d60) = 0x6028 0x003B (d59) = 0x8248 0x003A (d58) = 0x5032 0x0039 (d57) = 0x0000 0x0038 (d56) = 0x0006 0x0037 (d55) = 0x001E 0x0036 (d54) = 0x3400 0x0035 (d53) = 0x0069 0x0034 (d52) = 0x5000 0x0033 (d51) = 0x40C0 0x0032 (d50) = 0x01C0 0x0031 (d49) = 0x0013 0x0030 (d48) = 0x1A05 0x002F (d47) = 0x0280 0x002E (d46) = 0x0000 0x002D (d45) = 0x4F80 0x002C (d44) = 0x0318 0x002B (d43) = 0x0051 0x002A (d42) = 0x0002 0x0029 (d41) = 0x0000 0x0028 (d40) = 0x0000 0x0027 (d39) = 0x0000 0x0026 (d38) = 0x0000 0x0025 (d37) = 0x0000 0x0024 (d36) = 0x0000 0x0023 (d35) = 0x0028 0x0022 (d34) = 0x0000 0x0021 (d33) = 0x0000 0x0020 (d32) = 0x0000 0x001F (d31) = 0x0000 0x001E (d30) = 0x0030 0x001D (d29) = 0x0000 0x001C (d28) = 0x0000 0x001B (d27) = 0x0004 0x001A (d26) = 0x0000 0x0019 (d25) = 0x0400 0x0018 (d24) = 0x091C 0x0017 (d23) = 0x2406 0x0016 (d22) = 0x00A2 0x0015 (d21) = 0x0503 0x0014 (d20) = 0x0000 0x0013 (d19) = 0x0000 0x0012 (d18) = 0x0000 0x0011 (d17) = 0x26C4 0x0010 (d16) = 0x921F 0x000F (d15) = 0xA037 0x000E (d14) = 0x0000 0x000D (d13) = 0x0000 0x000C (d12) = 0x0000 0x000B (d11) = 0x0000 0x000A (d10) = 0x0000 0x0009 (d09) = 0x274C 0x0008 (d08) = 0x0001 0x0007 (d07) = 0x0C2D 0x0006 (d06) = 0x0DEC 0x0005 (d05) = 0x0008 0x0004 (d04) = 0x0000 0x0003 (d03) = 0x0200 0x0002 (d02) = 0x0000 0x0001 (d01) = 0x7652 0x0000 (d00) = 0x2000
Two things I notice. Register 0 is 0x2000. Pretty sure it should be 0x1000. Register 3 indicates a CRC fault. Not sure this is normal.
I have a configuration I developed in TICS Pro. I export the register settings and try to write them to the CDCE6214. The third column is the read back value after writing the value from the second column to the address in the first column.
0x0053 = 0xFD00 0xFF00 0x0052 = 0x01C0 0x05C0 0x0051 = 0x0004 0x0004 0x0050 = 0x0000 0x0000 0x004F = 0x0000 0x0000 0x004E = 0x1000 0x1000 0x004D = 0x0000 0x0000 0x004C = 0x0188 0x0188 0x004B = 0x8008 0x8008 0x004A = 0xA181 0xA181 0x0049 = 0x0000 0x0000 0x0048 = 0x0006 0x0006 0x0047 = 0x0006 0x0006 0x0046 = 0x0008 0x0008 0x0045 = 0xA181 0xA181 0x0044 = 0x0000 0x0000 0x0043 = 0x0006 0x0006 0x0042 = 0x0006 0x0006 0x0041 = 0x0808 0x0808 0x0040 = 0xA181 0xA181 0x003F = 0x0000 0x0000 0x003E = 0x0006 0x0006 0x003D = 0x0000 0x0000 0x003C = 0x6008 0x6008 0x003B = 0x8008 0x8008 0x003A = 0x502C 0x502C 0x0039 = 0x0002 0x0002 0x0038 = 0x0006 0x0006 0x0037 = 0x001E 0x001E 0x0036 = 0x3400 0x3400 0x0035 = 0x0069 0x0069 0x0034 = 0x5000 0x5000 0x0033 = 0x40C0 0x40C0 0x0032 = 0x01C0 0x01C0 0x0031 = 0x0013 0x0013 0x0030 = 0x1A14 0x1A14 0x002F = 0x0A00 0x0A00 0x002E = 0x0000 0x0000 0x002D = 0x4F80 0x4F80 0x002C = 0x0318 0x0318 0x002B = 0x0051 0x0051 0x002A = 0x0002 0x0002 0x0029 = 0x0000 0x0000 0x0028 = 0x0000 0x0000 0x0027 = 0x0000 0x0000 0x0026 = 0x0000 0x0000 0x0025 = 0x0000 0x0000 0x0024 = 0x0000 0x0000 0x0023 = 0x0028 0x0028 0x0022 = 0x0000 0x0000 0x0021 = 0x0000 0x0000 0x0020 = 0x0000 0x0000 0x001F = 0x0000 0x0000 0x001E = 0x0030 0x0030 0x001D = 0x0000 0x0000 0x001C = 0x0000 0x0000 0x001B = 0x0004 0x0004 0x001A = 0x0000 0x0000 0x0019 = 0x0400 0x0400 0x0018 = 0x0718 0x0718 0x0017 = 0x0406 0x2406 0x0016 = 0x00A2 0x00A2 0x0015 = 0x0503 0x0503 0x0014 = 0x0000 0x0000 0x0013 = 0x0000 0x0000 0x0012 = 0x0000 0x0000 0x0011 = 0x26C4 0x26C4 0x0010 = 0x921F 0x921F 0x000F = 0xA037 0xA037 0x000E = 0x0000 0x0000 0x000D = 0x0000 0x0000 0x000C = 0x0000 0x0000 0x000B = 0x0000 0x0000 0x000A = 0x0000 0x0000 0x0009 = 0x0000 0x274C 0x0008 = 0x0001 0x0001 0x0007 = 0x0C0D 0x0C2D 0x0006 = 0x0E2C 0x0DEC 0x0005 = 0x0008 0x0008 0x0004 = 0x0040 0x0040 0x0003 = 0x0000 0x0000 0x0002 = 0x0000 0x0000 0x0001 = 0x2660 0x2660 0x0000 = 0x100C 0x2000
You can see here address 0 did not change. I know the reset bit should clear itself, but the GPIO directions still seem incorrect.
I can also read the EEPROM. Here are those results if it helps.
EE Addr 0x0000 (00) = 0x7002 EE Addr 0x0001 (01) = 0x487F EE Addr 0x0002 (02) = 0x1B12 EE Addr 0x0003 (03) = 0x0000 EE Addr 0x0004 (04) = 0x28A0 EE Addr 0x0005 (05) = 0x4CD0 EE Addr 0x0006 (06) = 0x0700 EE Addr 0x0007 (07) = 0x6680 EE Addr 0x0008 (08) = 0x8320 EE Addr 0x0009 (09) = 0x5A24 EE Addr 0x000A (10) = 0x6C24 EE Addr 0x000B (11) = 0x122D EE Addr 0x000C (12) = 0x1626 EE Addr 0x000D (13) = 0x4909 EE Addr 0x000E (14) = 0x0434 EE Addr 0x000F (15) = 0x0102 EE Addr 0x0010 (16) = 0xA801 EE Addr 0x0011 (17) = 0x00EC EE Addr 0x0012 (18) = 0x4000 EE Addr 0x0013 (19) = 0x2470 EE Addr 0x0014 (20) = 0x0200 EE Addr 0x0015 (21) = 0x0060 EE Addr 0x0016 (22) = 0x0000 EE Addr 0x0017 (23) = 0x0000 EE Addr 0x0018 (24) = 0x0000 EE Addr 0x0019 (25) = 0x0A22 EE Addr 0x001A (26) = 0x1800 EE Addr 0x001B (27) = 0x00D8 EE Addr 0x001C (28) = 0x8000 EE Addr 0x001D (29) = 0x0C40 EE Addr 0x001E (30) = 0x0000 EE Addr 0x001F (31) = 0x0C48 EE Addr 0x0020 (32) = 0x0000 EE Addr 0x0021 (33) = 0x0D08 EE Addr 0x0022 (34) = 0x0000 EE Addr 0x0023 (35) = 0x1008 EE Addr 0x0024 (36) = 0x0000 EE Addr 0x0025 (37) = 0x0000 EE Addr 0x0026 (38) = 0x0000 EE Addr 0x0027 (39) = 0x1000 EE Addr 0x0028 (40) = 0xA440 EE Addr 0x0029 (41) = 0x00EC EE Addr 0x002A (42) = 0x4000 EE Addr 0x002B (43) = 0x2470 EE Addr 0x002C (44) = 0x0200 EE Addr 0x002D (45) = 0x0060 EE Addr 0x002E (46) = 0x0000 EE Addr 0x002F (47) = 0x0000 EE Addr 0x0030 (48) = 0x0000 EE Addr 0x0031 (49) = 0x0A22 EE Addr 0x0032 (50) = 0x1800 EE Addr 0x0033 (51) = 0x00D8 EE Addr 0x0034 (52) = 0x0000 EE Addr 0x0035 (53) = 0x0C50 EE Addr 0x0036 (54) = 0x0000 EE Addr 0x0037 (55) = 0x0C50 EE Addr 0x0038 (56) = 0x0000 EE Addr 0x0039 (57) = 0x0D10 EE Addr 0x003A (58) = 0x0000 EE Addr 0x003B (59) = 0x1100 EE Addr 0x003C (60) = 0x0000 EE Addr 0x003D (61) = 0x0000 EE Addr 0x003E (62) = 0x0000 EE Addr 0x003F (63) = 0x0000
I notice the CRC register is all 0's so it is probably no wonder the CRC compare is failing.
I am stuck. I have tried several things but I can't get it to generate the required outputs. It seems like a programming problem. Have you seen anything like this?