Part Number: LMX2594
I have implemented two LMX2594 devices into a design and on multiple boards this works, but one board is failing where one of the LMX devices fails to lock. I have verified that all the passive components on the loop filter seem to be correct. All power pins have been probed and a steady 3.3V is getting to every power pin, we can communicate with the device via I2C and read and write registers, but I have noticed that all the bias voltages (pin, 3, 27, 29, 33, 36, and 38) are either a very low voltage that is not correct, or they are 0V. I cannot find any shorts to ground on any pins and I cannot figure out what could cause this type of failure. I need help understanding what would cause these bias voltages to be so incorrect and cause the part to be dysfunctional.