Part Number: LMX2595EVM
Hi Team,
The output path is configure as differential and understand if using single ended, we need to add a pull up resistor/inductor. I try out with the EVM board, if the unused port (-ve) terminated with 50ohm terminator the output power at (+ve) drop by 1 dB. So, what is the recommendation from TI or can i just leave the port open? What is the impact if the other port just left it open (only pull up resistor). Measurement done with SA shown no different in term of Spur and Phase Noise.
Beat Regards,
Tom Liu