Part Number: LMH1983
Other Parts Discussed in Thread: LMH1981
Hi
We referenced the Figure 22 in the datasheet as a typical application of genlock mode and designed a custom board.
The timing signals (H/V/F) from LMH1981 are buffered with a FPGA once, then coming to LMH1983.
That because we suppose to select either free-run mode (no input timing signals from FPGA) or genlock mode (with H/V/F signals from FPGA).
Then, we have some questions.
1. When we work LMH1983 as the free-run mode, do we all have to do is setting registers like Table 13?
2. When does NO_LOCK assert in the free-run mode?
3. Is it possible to change the free-run mode to the genlock mode with the same circuit?
4. If answer to question 3 is yes, is it enough to change the register settings from Table 8 to Table 13?
5. If answer to question 3 is yes, is there a recommended sequence to change the register settings for each mode?
BestRegards