Part Number: LMK04828
Other Parts Discussed in Thread: LMX2572, LMX2582, LMX2594, LMX2820, LMK04832
.... This is more of a general JESD204b question....
Hello -
All of the JESD204B compliant Dual PLL devices (LMK04828 is the one I've used in the past) have integer N dividers in PLL2. What's the reason behind this? Is it for simplicity, spurs, phase noise, etc. Classic integer vs fractional reasons. Or is there more to it? Maybe a fractional N-divider's SDM causes issues with a JESD DCLK+SYSREF pair re-timing and latching? Or something else?
The reason I'm asking is that I'd like more flexibility of my JESD204 clock generation. I'd like to not be limited to PLL2's PFD rate and I think a good solution would be an external fractional synthesizer (maybe LMX2572 or LMX2582) into the Fin of the LMK04828. I'd then only use the LMK04828 as a fanout chip.
I'm wondering (from a JESD204b system perspective) if the VCO needs to be an integer synthesizer or can it be fractional.
Thanks for the support.
Chris H