This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Request for Output power vs OUTA_PWR specs At different frequencies

Genius 9880 points
Part Number: LMX2594

Hi Team,

A customer is requesting if we have existing data or if we can provide a data of Output Power Normalized To Maximum Across
OUTA_PWR With Resistor Pullup at 13.5GHz to 15GHz range. Thank you and looking forward for your responses.

  • Hello,

    Unfortunately we do not have data on this for each range of frequencies. However following the datasheet recommendation I would use OUTx_PWR = 15 in the 13.3 GHz to 14.3 GHz region to avoid drops in power at hot temperature.

    Please follow suggestions in datasheet "Table 10. OUTx_PWR Recommendations for Resistor Pullup"

    Thanks,

    Vibhu