This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ32002: Swtichover voltage

Part Number: BQ32002

Hi all,

I got a question about swtichover voltage of this device. In the datasheet, the switchover voltage of Backup -> Operating is 2.4V. However datasheet 7.3.2 indicates that the switchover of Vback -> Vcc when Vcc is either Vback or Vref (1.8V). Considering this, the switchover Backup -> Operating is same as Operating -> Backup, i.e. 1.8V. What does this 2.4V come from?

Also, do you have any distribution data of Vref? The switchover voltage when Vback<Vref is Vref, so I need the data to decide the design parameter of switchover voltage.

Regards,
RYO