Hi All,
my customer is looking for a new PCIe Clock Generator Gen-1, 2, 3 . Also new generations are ok, if are not too expensive.
Below the main specs:
- PCIe Clock compliance gen 1, 2 or greater.
- Input: 25MHz from crystal quartz and CMOS 3.3 25MHz
- Output: at least 4 differential output HCSL 100MHz
Currently they are using the IDT 5V41065 with 2 output HCSL. As written above for this redesign 4 diff. output HCSL are mandatory.
Target cost: less than 1$. They are also considering the competition.
If you would like to take this offline, please let me know.
Thank you
Riccardo