Part Number: LMX2595
Other Parts Discussed in Thread: LMX2594EVM, , TIDA-01410, TICSPRO-SW
Hello.
I have few queries regarding LMX2595.
1) The lock time of LMX2595 is calculated by using PLLatinum sim tool. But for the frequencies higher than 15GHz what could be the lock time. I mean once the VCO frequency is doubled what is the effect on lock time.
2) While programming LMX2595 it is recommended to transfer MSB first. Now in that case lets consider I need to transfer 0X00251C. So, Should I program to transfer 1C at the beginning.
3) I am trying to replicate the design with eliminating the additional connectors. Any PCB guidelines and gerber files for reference.
4) The output power level at high frequencies is very less. Is it desirable to use a Low Noise Amplifier at the output of LMX2595 to attain the desired power level.
Thanks in Advance.