Hi,
We are currently using LMK05318RGZT in our board and we are trying to produce an output clock identical or as close as possible to the input clock.
We have 48MHz crystal on board that drives the XO input of the LMK05318
Using the TICS Pro software, we are able to see that LOPL_DPLL and sometimes LOFL_DPLL are set. Occasionally they are not.
I found that with adjusting the DPLL Frequency and Lock Detect Thresholds, I can sometimes get a clean signal (no LOPL_DPLL, no LOFL_DPLL).
Other times it will not work unless I toggle between PRIREF and SECREF. When I toggle, the DPLL is somehow able to lock onto the incoming clock (both LOPL_DPLL and LOFL_DPLL are cleared).
How can I make it so that neither LOPL_DPLL or LOFL_DPLL are never set? Why would LOPL_DPLL or LOFL_DPLL lock on when toggled?
Thank you for your help and I hope to hear back from you soon.
-Gavin