Part Number: BQ4802Y
Other Parts Discussed in Thread: BQ32000, BQ32002, BQ4802LY
I have a circuit exactly based on the PDF Datasheet on Page 1 HERE
The issue is that when I set the time, for example if I set it at 12:00:00 it will never cycle, never count's up the seconds or changes. It remains at that time forever!
I have replaced the 32.768kHz crystal but that has not solved the issue.
I suspect a bad lot of chips.
This is because I ordered 3 of the same chips from TI before and had no issues on the same circuit. I took one of the known good ones off a PCB and replaced it with the a new one from the lot with the issue and that board no longer works. I put the known good one onto the board that was not working from the new lot and it works.
TI thinks it's an application issue. But I don't buy it. I ordered 25 of these things and after 5 fails I stopped soldering and they will not approve my return.
Can anyone offer any suggestions of why the chip will not keep cycle the time? The battery that keeps the backup power is a 3v CR2032.
Thanks in advanced!