I am using the LMK04828 with a 5MHz reference to generate 100MHz from PLL1, then using PLL2 to generate 325MHz. I have gotten a design working in cascaded mode (PLL1 feedback from OSCin).
My problem is that when I attempt to set the LMK04828 to zero delay mode (PLL1 feedback from DCLK6 or DCLK8) PLL1 never locks. PLL2 is locked in both cases. In both cases CPout1 is appox 1.65V, does this suggest a false loss of lock report?
The only change to the working design was to set PLL1_NCLK_MUX to take input from FB_MUX and change the PLL1_N from 10 to 65. I have confirmed that I have the FB_MUX_EN bit set high in both cases.
What could be causing this problem?