Part Number: TLC555
Hi,
My customer wants to count about 2 minutes with TLC555. To achieve this, you must have multiple resistors in series and multiple capacitors in parallel. Are there any concerns when doing this?
For example, when the time constant is 100 seconds, I think that the theoretical time constant will be the same when R is 10 MΩ and C is 10 μF, and when R is 1 MΩ and C is 100 μF. Do you recommend which value?
Thanks and best regards,
M.HATTORI.