Other Parts Discussed in Thread: SA555, LM555, LMC555
Hi,
My customer uses TLC555IDR, instead of SA555DR.
*1. According to datasheet of SA555, A bypass capacitor is highly recommended from VCC to ground pin; ceramic 0.1 µF capacitor is sufficient. In other hands, on the TLC555 datasheet, Minimum recommended is 0.1-μF ceramic in parallel with 1-μF electrolytic.
Why is different?
Is the noise immunity of TLC555IDR weakened when comparing the bipolar IC and the Cmos IC?
*2. On 1uF electrolytic capacitor on TLC555, What characteristics do you need in a capacitor?
*3. Regarding the type of capacitor of TLC555, is it possible to use other than electrolytic capacitors?
Please advise us.
Thanks and best regards,
M.HATTORI