Hi all,
I'd like to get an output clk locked with SECREF, I use the TICS-Pro to generate reg settings, now I let,
XO=24.576MHz (50ppm), SECREF=1Hz-1MHz(from Agilent 33210A Waveform Generator), OUT7 = SECREF * 10
It works well for input freq large 100kHz, the output7 sync with the input.
It doesn't work for input below 100kHz, the output7 freq is right, but doesn't sync with input, is there anything I should pay attention?
Thanks,
Jiahua