Part Number: LMX2594
Hi,
I'm using a LMX2594 to generate a clock and a Sysref signal. I'm generationg a
burst of 5 sysref impulses. In this case the AC coupling is not a good idea and I want to use the DC
coupling. The Rx is a PI6C5916004ZHIE and the maximum Vih is VDD-0.9 = 2.4V.
I don't connected directly the RF_outB of the LMX2594 to the Rx. Can I reduce the
OutB high level of the LMX2594 removing the Cap and inserting a resistor?
Do you have any suggestion to adapt the 2.3-3.3V to the input levels of the PI6C5916004ZHIE?
Thanks you in advance for your attention.